如题,BQ769x0的VSS必须接BAT-吗?
我的设计是一块板上集成Charger、Monitor(就是BQ769x0,不用CHG、DSG引脚),统一用MCU进行监视管理。现在Charger和Monitor的VSS之间有充电电流检测电阻Rsns,有电位差。BQ769x0的VSS能否接到Rsns的PACK-侧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,BQ769x0的VSS必须接BAT-吗?
我的设计是一块板上集成Charger、Monitor(就是BQ769x0,不用CHG、DSG引脚),统一用MCU进行监视管理。现在Charger和Monitor的VSS之间有充电电流检测电阻Rsns,有电位差。BQ769x0的VSS能否接到Rsns的PACK-侧?
谢谢答复。
如果charger 和 9x0 各自有独立的MCU,有多大的电位差也没问题。但是否可以只用一个MCU,而且控制接口直连?
如果VSS接到PACK-侧,VC0的电位将不为0,对VC1的值会有影响吗?对其它功能会有影响吗?
1. 可以
2. VC0如果不为0 会对VC1的测量带来误差。另外如果电流尖峰在电阻上形成的压差超过-0.3V有可能损坏芯片。