辅电和开环调试都正常,开环调试给定一个固定的移相角随着输入电压的慢慢增大,输出电压也增大,但是闭环调试时发现输出电压要么4V左右,要么就115V,改变软启动时间可以改变这个输出电压,要么就是4V,要么就是115V,运放上的闭环反馈怎么调也没有用,基准2.5V是准的,我是做恒压点80V,负载为20R,拓朴为移相全桥,前面一级电路是PFC电路移相全桥的母线电压是380V左右,..现有原理图一份,不知道是哪里出了问题,请TI工程师们帮忙看看
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
辅电和开环调试都正常,开环调试给定一个固定的移相角随着输入电压的慢慢增大,输出电压也增大,但是闭环调试时发现输出电压要么4V左右,要么就115V,改变软启动时间可以改变这个输出电压,要么就是4V,要么就是115V,运放上的闭环反馈怎么调也没有用,基准2.5V是准的,我是做恒压点80V,负载为20R,拓朴为移相全桥,前面一级电路是PFC电路移相全桥的母线电压是380V左右,..现有原理图一份,不知道是哪里出了问题,请TI工程师们帮忙看看
根据你的描述还是闭环反馈的问题。
你测量一下反馈点的电压,
第一,要保证逻辑的正确性,即是否为负反馈
第二,看看电压值是否在芯片管脚的要求范围内
波形好像没显示出来,最好结合原理图再描述一下
likai wang 说:各位大哥,请帮看看,我用UCC3895+倍流整流方式做的,输入DC48V,输出DC12V,2个储能电感没共起来是这样的波形,共起来后就变成这样了,输出电压只有10V左右了
看两个波形叠起来后怎么也有17,8V啊?怎么只有10V输出呢?