该芯片按照手册的典型应用电路连接调试接,输入电压为5v,工作电流为0.5安培,输入端正负极之间串一个2.2uf的电容,输出端怎么是6v电压?如果去掉这个2.2uf电容后,输出电压变为0v。电路图如图片所示。怎样才能使输出端电压为5v?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
接上电容,带上一点负载,输出电压就是5V,因为这种电源是开环控制的,如果需要很准的电压,建议后接一个LDO。
Hi
此芯片内置LDO, 输入5V/0.5A吗? 这个功率很大啊
输出带不带在都不应该到6V, 芯片可能已经坏掉了。
layout上注意输入输出电容尽量靠近芯片输入输出脚。