This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

<求助>BQ27441 RUP_DIS不复位

Other Parts Discussed in Thread: BQ27441EVM-G1A

你好

 最近使用BQ27441EVM-G1A进行电池的学习。有如下疑问:

1.我在Parameter Q&A里设置termination voltage 2750mV,但是在learning cycle中,termination voltage为2900mV,而且这是最小值。

2.开启learning cycle开始学习,提示我放电,这里我直接接一个电阻放电,电流在450左右,但是会变动。等到电压低于2900mV,提示我移除负载,之后等待RUP_DIS复位,可是我等了6小时还是没有复位,直接退出了。(共有5次测试,只有1次成功复位,耗时16分钟左右)

3.基于上次成功复位后,开始充电,可是冲到100后,FC没有置位,一直冲,直到充电电流20mA时还没有置位。

4.是否放电也需要恒流放电?

谢谢!