This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The voltage level on EN/TOFF also programs the EN/TOFF 2 I minimum off-time (TOFF) for the controlled MOSFET. EN/TOFF is internally driven by a two-level current source, so the voltage level on EN/TOFF can be set by connecting a resistor from EN/TOFFto GND.
The data sheet of the chip describes that when REN / TOFF takes between 70-80KΩ, VEN switches between 1.4V-0.8V, that is to say this time the chip should be in the enable and disable switching state, but in the datasheet that is “For any 70 kΩ < REN/TOFF < 80 kΩ, VEN toggles rapidly between 1.4 V and 0.8 V and the device remains disabled. In this situation, average ICC is approximately half of the normal run-mode current, ICC(on).”.