This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:最近打算用LM5085设计一款电源,有什么需要注意的地方?

Other Parts Discussed in Thread: LM2576HV, LM5085, LM5161

最近打算用LM5085设计一款电源模块,平常48V输入,24V输出,输出电流最大1A。因为输入电压的波动比较大,可能会到60V以上,所以不能用LM2576HV,才想用LM5085的,但是之前没用过这个芯片,不知道在设计过程中需要注意什么。我看TI官网的设计软件里推荐的输出电容,使用的是TPSE156K050R0250这个电容,成本很高,我想问下这个地方必须用这个电容吗?用一般的高频铝电解电容可以吗?

  • 看官网上有一款LM5161的电源芯片,这个芯片设计起来是不是比5085要简单一点?这个芯片网上的资料特别少

    • 输入电压的波动较大,可以在输入级加一个LC滤波电路
    • 输出电容不是必须选择这款,铝电解电容在温度稳定性,ESR和ESL方面的特性都略低于钽电容,另外,不同的电容对电源环路的影响会不一样,所以更换电容后还需测试一下