1.8V的输入,需要1.1V的输出,我在官网上找到了TPS7A7001和TPS7A7002这两款LDO,我需要1.1V的电流至少是1.1A。请问这两款芯片哪个性能更好?
因为TPS7A7001手册里面是380 mV Dropout Maximum at 2 A,我这边有700mV的压降,是不是只能做到最大1.08A的输出,似乎是不能满足我的要求?
请高手帮忙解读一下。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.