This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24715EVM无法进入充电

Other Parts Discussed in Thread: BQ24715

我在申请了一块BQ24715的EVM板,在测试时,ACIN=20V,sys带载0.7A,CELL=float时,BAT接电池后,无法进入充电。输出8.96V。没找到原因,希望能有人帮忙解答。

  • 用TI的BQ studio,看下charge Enable寄存器位是否没有打开。

  • 你好,BQ24715 BATFET的控制模式中,disable LDO mode的目的是为啥?感觉很多余啊?

    在补电模式中,DS中写要大于256mA才能打开BATFET,但是demo测试中并未看到,BATFET电流小于256mA时就已经打开,这是什么情况啊?

    EC talbe中有个light load 比较器,写着当进入轻载模式时,LS 管不会打开,但实际测试仍然会打开,芯片对这个轻载比较器的真正响应是怎么样的?

    感谢。