This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50怎么通过设置电池容量百分比 来实现断电



请教一下各位,鄙人想让电池放电在1%的时候就断电,不是通过设置电池电压低于多少V的时候来断电,请问该如何设置,

  • 您好,能先请教下您为什么会希望做这样的设置吗?

    对于电池来讲,在放电时会SOC会受很多因素的影响,比如放电电流,温度等。因此,在不同放电电流下SOC为1%在电量上来讲对于电池是差异很大的,此时的剩余电量在不同放电电流下差别也很大。这也就是为什么一般通过设置放电最低电压来设置断电的原因。

  • 哥们,我是这样想的,参考这个图

    电池在放电的时候,不同负载装状态下,电压是不一样的,比如说当我在比较重的负载情况下,我设置的断电电压为3200mv,此时显示SOC为0%刚好断电,

    但是如果我在轻负载的情况下(不进行WiFi传输,硬件编解码等等),那么在SOC显示为0%的时候却没有断电,系统可能还要运行一段时时间,等电压低于

    3200mv,才能断电,也就是说当电池计量SOC显示为0%的时候不会立刻断电。

    我现在想明白了,我还是得到系统层去做这个事情,毕竟BQ40只是一个电池计量计而已,要求不能这么高。。。。