选择一个隔离芯片 (DC-DC)要求就是这个芯片输入5V, 可以达到5路,每一路都是5V,这5路是相互独立,输出电流的范围6mA-20mA 范围内,假如有12-12V(DC-DC),或者其他电压的多路隔离也可以 谢谢回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
5V到5V隔离电源可以使用TPS55010,详见
变压器具有5个匝数一样次级绕组就可以实现5路5v隔离输出。参照参考设计
关于附边能绕多少个绕组出来,您需要问下电感(变压器)厂商, 常见的是1~2个,输出电流很小,您可以尝试采用多个变压器并联,由TPS55010作为主芯片来转换。
或者您可以用DCV010505: www.ti.com.cn/.../getliterature.tsp 这样的无反馈隔离1w的电源芯片来实现。