This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问uc2909-ep 和 bq24450的区别

Other Parts Discussed in Thread: UC2909-EP, BQ24450

您好:请问uc2909-ep 与bq24450的主要区别是什么?

我公司要为三相永磁交流发电机配套稳压电池充电器,电机输出ac0v-90v输出电压值可调低,对于28.2V15A的具有温补的恒压恒流两阶段78AH铝酸电池充电,UC2909-EP和bq24450选用哪个更好?另外如何确定其输入电压需要高于输出多少才合适?谢谢。

  • Hi,

    UC2909-ep是开关类型(PWM驱动)charger,更适合大电流应用。bq24450是线性的,大电流下效率低,调整管发热高。UC2909最大输入电压只能到直流40V,最大占空比典型值为95%,所以输入允许的最小值为28.2V/0.95=29.68V。

  • 急!谢谢您的回复。我决定采用UC2909EP方案,我还有两个问题需要向您咨询,

    一,请问我是否可以选择UC2909的输入电压从直流输入Vdc分压得到以降低最大110直流输入?还是只能用隔离变压器降压后将buck的输入与uc2909的供电并联的形式?

    二 uc2909ep国内没有现货,只能TI官网可以购买小批量的,请问如果产品定型为UC2909EP是否能保证后期的产品供货呢?如果不能,BQ24450也不合适,您还可以为我推荐一款别的合适的产品和方案吗?

     项目周期短,期盼您的解答,非常感谢。

  • Hi,

    一,请问我是否可以选择UC2909的输入电压从直流输入Vdc分压得到以降低最大110直流输入?��是只能用隔离变压器降压后将buck的输入与uc2909的供电并联的形式?

    不推荐分压,推荐隔离buck降压。

    二 uc2909ep国内没有现货,只能TI官网可以购买小批量的,请问如果产品定型为UC2909EP是否能保证后期的产品供货呢?如果不能,BQ24450也不合适,您还可以为我推荐一款别的合适的产品和方案吗?

    UC2909EP还是在量产中,不会EOL,请选择我们正规的代理商渠道或TI官网小批购买。

  • 谢谢您的回复,请问不推荐分压的原因是什么,另外有无隔离BUCK的参考设计可以推荐,谢谢。

  • 隔离BUCK在datasheet上看是fly back拓扑,这种拓扑只能应用于小功率,如何用隔离拓扑实现大功率,对此困惑