Other Parts Discussed in Thread: LMZ23610
现采用2片LMZ23610并联的设计,输出5V。
供电输入带有电池,因此电压会有跳变的情况,最大跳变为8V到24V,差值达16V。这对5V输出会有什么影响没有?
原理设计已经做完了,有这么个担心。在想是否需要在输入端加稳压电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.