用TPS23861搭了一个PSE供电电路,用着用着芯片和mosfet烧了,具体现象:
1)供电异常,I2C无法访问;
2)更换TPS23861芯片,detect结果显示mosfet fault;
3)更换mosfet,可以正常供电。
具体什么情况下烧坏的,没有看到现场。
有人有碰到过这种问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
4块板子三块正常一块不正常,建议多做比较,包括Layout以及焊接。
其次零件上建议做交互验证,例如电感等重要器件。(一般容易造成烧的原因都是layout的短路,过压过流,电感饱和等,逐一排查)
好的板子也会出现芯片3.3V击穿问题。不是只有一块,好板子用着用着就挂啦。无过冲过压。目前在芯片的3.3V增加限流电阻,好像也不理想