This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于变压器的问题

Other Parts Discussed in Thread: UCC28950, UCC25600

你们用的开关电源,做600w左右的,开关频率一般用多少? 比如说半桥,选择多少频率的变压器?  TI有这样的电源,频率做到2M的么?

  • 这么大的功率,一般做在50kHz以下。频率做得高了,开关损耗会太大。

  • 您好,

      600W的功率看您选择什么样的拓扑。

      TI有普通半桥,全桥的方案,这种一般选择50K左右的开关频率。

      如果选择准谐振型的如移相全桥,可以开关频率更高值100kHz左右, UCC28950。

      如果选择谐振型如LLC,开关频率可以更高如300kHz, UCC25600。

      开关频率多高还取决于驱动器件,布板,效率折中等因素。2M的600W电源可以考虑采用LLC拓扑,数字控制器配合变压器驱动方式去做。您在IEEE上可以搜到类似博士论文,谢谢

    Regards,

    Patrick

  • 你好,

    看你做的是什么电路,比如半桥LLC 600w的,开关频率一般都做到百K级别的。

  • 看你的技术水平,如果新手建议你选择普通的全桥,开关频率控制在100K以内,如果是老手,可以用LLC或移相全桥,开关频率响应的可以高一些。