This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24617充电时间误差异常

现象:电池放电放空,给电池充电,充电超过10个小时也只能充到70%-80%

TTC脚的电容取值为68nF,理论充电时间6.35小时

用ev2300监控充电过程发现不到4个小时电流从恒流模式变为0,此时充电电路不工作。电容从pcb取下测量在64nF 材质为x7r 50v  0603

将TTC脚的电容取值设置为100nF,能完成整改充电过程。请教下,还有什么原因可能引起这个问题。