This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:关于TIBQ34z100大电流容量跳变

Other Parts Discussed in Thread: BQ34Z100, BQ34Z100-G1

描述如下:

                   采用18650-10S3P  ,36V9Ah,电芯三星18650 30Q,支持倍率放电,在20A放电时,容量百分比出现跳变,log数据截图如下:

DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags 

 14:20:52,464.000,0x0016,0x0003,77,100,6306,8297,37250,-19949,-19950,30.3,19,65535,2307,-7432,55.1,3,94,42000,4500,0x0961,0x0111,0x0400,2,4,0,831,6300,8297,499,1166,14,1512,712,1164,14,938,SUCCESS

117,2016-11-21 14:20:56,468.000,0x0016,0x0003,0,100,0,2008,37220,-19949,-19951,30.1,0,65535,0,-7429,55.2,3,94,42000,4500,0x0961,0x0117,0x0400,3,4,0,831,-11,2008,503,1188,14,1512,712,1186,14,938,SUCCESS

TKS