1、按照芯片手册中R1、R2进行12v转5v设计,结果经调试发现,R1和R2居然是反的,请技术支持确认下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、按照芯片手册中R1、R2进行12v转5v设计,结果经调试发现,R1和R2居然是反的,请技术支持确认下,谢谢!
Hi
http://www.ti.com.cn/cn/lit/ds/symlink/lm2736.pdf 第16页, 这个计算没有错。
您好:
我知道公式没有错,但是实际使用发现焊接时R1和R2电阻就需要数值颠倒焊接,不拿到芯片测试是发现不了的,我也比较差异TI这个大厂会犯如此低级的错误。
输出和FB是R1,FB和地是R2。这个不可能错的,还请仔细确认
你好,没有任何推脱责任的意思,FB的理论值是1.25V,你可以测量一下。
如果下拉电阻一端电压是1.25V,一端是0V,那一定是没有问题的,否则基本的物理定律都不对了。
实际测量FB到地电压1.265V,符合预期,手册里面说
The output voltage is set using the following equation where R2 is connected between the FB pin and GND, and R1 is connected between VO and the FB pin. A good value for R2 is 10 kΩ.
也就是R2是接地电阻,R1是接电源电阻,R2推荐值为10k,我们需要5V输出,按照公式计算R2=10k,R1=30k,实际焊接测试发现输出电压值仅为1.6V左右,代入公式正好是R1、R2互换后的值,替换R1、R2顺序后电压为5V左右,一切正常,请问我还需要确认什么?
或者比如FB上串联一个1k左右的电阻,看上面是否有很大的压降?
上面打错了,不好意思
我也很好奇,所以还希望你通过我上面提到的方法进一步测试验证。看FB上是否有很大的电流(相比于R1和R2)
从芯片内部结构来讲,并不是简单的将某些东西弄反了就可以产生你描述的结果。谢谢
已经确认过了没有错,先这样用了,不想多说了,就当给后面用的人提个醒吧