您好:
使用TPS51200为DDR3的地址线控制线终端电阻提供0.75V的上拉供电。没连接负载时,输出VO为0.75V正常,而连接负载后输出电压被VO拉到0.13V左右。VLDOIN为1.5V,Vin为3.3v正常,REFIN和REFOUT都是0.75V,EN也是3.3V。测量负载的对地电阻为36.5K,而开发板的对地电阻为2K,设计都是按照开发板来的,请问可能是哪里出现问题,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.