目前使用LM3409HV驱动LED遇到输出电流控制问题如下:
输入是55V的开关电源,用来驱动不同串数并数的LED,有3种,具体参数如下图,
会出现正常点一段时间(几十分钟到十几个小时不定)后,LM3409HV失效,失效现象是:
1、PGATE脚不会正常控制外部FET,只会根据PWM高就导通FET,PWM低就关断FET,在PWM高,FET导通过程中,PGATE脚是无变化的全高状态
2、无法工作,PGATE无输出,FET永远无法导通
在这两种情况出现的时候,只要更换新的LM3409HV后,驱动又可正常工作仍然是几十分钟到十几个小时不定后出问题,我用来驱动以下三种有的多有的少一共20组LED,每次出问题的组不是固定的,没有规律可循
想请教各位,有没有什么解决问题的方向提供下,谢谢了!(是否可以怀疑LM3409HV本身的货源问题)
3种情况附图: