This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040给单节锂电池充电充不满问题

Other Parts Discussed in Thread: BQ24040

你好,

BQ24040给单节500mA锂电池充电时,会出现充十几个小时CHG依然为低电平(FET on),可能是什么原因?

这种情况容易出现在给完全放电的电池充电时,且若出现这种情况,重新拔插充电器,再充一小会儿就可以正常指示充满电。

电路负载平均电流3mA左右,会有10Hz、1ms宽、150mA左右的电流脉冲。

快速充电电流、终止充电电流如图所示,设为163.6mA、16.3mA。

请问偶尔出现的CHG一直不跳变的情况,会是什么原因?