This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计电流为 : 360mA
实际电流为: 700mA
请看图,有哪里不对吗?
亲;建议差下R9及其周围PCB。
R9取值如果没问题,建议查一下pcb
按照公式I=(1.24/0.3)*(1/11.5)=359mA 。但是R14这里,规格书有说明,这里有一个1.24V电压,ICSH=1.24/R14 ,如果这个ICSH电流大于100uA,则 ILED电流就不是1倍,这个规格书有一个线性图的比例关系。所以你计算出的300多毫安,实际不是的原因。只需要把R14值修改为12.4K,电流就是0.33A了。