要求输入:能提供3.3v、或5v、或12v,芯片能使用任一个输入电源就行
要求输出:变换到-45v左右,可能要根据负载器件具体微调;能有几mA电流负载能力就够了。
用途:给APD供电
其他:希望外挂器件不要太多太大哈^_^
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
很多boost芯片都可以,做一个 负输出,然后增加一到两级的chargepump, 正输出做反馈。
外围器件还好,工作频率是1.2M,有没有工作频率高一些的?滤波好处理一些
1.6M HZ开关频率的LMR64010可以看看
你好,这款芯片是升压芯片,我们的应用场景是希望得到反向的高压(也是给APD供电)
你好,64010这款芯片是升压芯片,我们的应用场景是希望得到反向的高压(也是给APD供电)
Hi
上面的TPS61170改一下反馈电阻不就行了吗?
Hi
升压芯片加chargepump可以得到负电压的。