最近需要做一个锂电池的供电模块,要求如下
电池电压:8.4
输出电压:9V左右
输出电流:1A
有充放电保护功能
同时与用电器接入电网,有电时电池充电,停电时,电池给用电器供电。
效率暂时不考虑。
求推荐TI官网可以提供样片的充电控制IC,效率比较高的效率一般的最好都有。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个要求可能需要用多个芯片去实现,可以用一个充电芯片+一个升压芯片+两个二极管去做,输入电压和boost分别用二极管去给负载供电,充电芯片可以考虑BQ24133,升压芯片可以选用TPS61088,如果需要自动切换TPS61088的使能管教用输入电压反向去控制