This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24093的TS管脚问题



TI的工程师你们好!

我现在使用贵司的该款电池管理芯片给我一个手持设备充电用,设备的供电电池采用单节锂电池,内部引出了100k的NTC管脚TS用来监测电池温度。充电管理部分的电路图如下:

现在的问题是,当电池的TS与BQ2903连接时,测得TS脚电压为1.5V左右,电池不能被充电,即使电池耗电导致电压降到过放电压3V关断输出时,充电芯片都没有给电池充电(前端测5V输入电流为0),实测CHAGRE脚为高电平,PG脚为低电平;当我断开电池的TS时,测得2903的TS脚为1.9V左右,这时电池可以正常充电,充电电流100MA左右,CHAGRE脚和PG脚均为低电平,但是奇怪的是这个precharge电流100MA维持了很久一直没进入快充(大改30分钟)。请问,这个TS脚这种情况电压正常吗?可能是什么问题?谢谢!