This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMC检测主要项目



深圳立讯检测有专业的实验室,TUV机构都常来我们实验室测试,EMC检测主要项目有:

空间辐射(Radiation): EN55011,13,22 FCC Part 15&18, VCCI

传导干扰(Conduction): EN55011,13,14-1,15,22, FCC Part 15&18, VCCI
喀呖声(Click): EN55014-1

功率辐射(Power Clamp): EN55013,14-1
磁场辐射(Magnetic Emission): EN55011,15
低频干扰(Low Frequency Immunity): EN50091-2
静电放电(ESD): IEC61000-4-2、EN61000-4-2、 GB/T17626.2
辐射抗扰度(R/S): IEC61000-4-3、 EN61000-4-3 、GB/T17626.3
脉冲群抗扰度(EFT/B): IEC61000-4-4、EN61000-4-4 、 GB/T17626.4
浪涌抗扰度(SURGE): IEC61000-4-5、 EN61000-4-5、 GB/T17626.5
传导骚扰抗扰度(C/S): IEC61000-4-6、 EN61000-4-6 、GB/T17626.6

工频磁场抗扰度(M/S): IEC61000-4-8、 EN61000-4-8、GB/T17626.8
电压跌落(DIPS): IEC61000-4-11、 EN61000-4-11、 GB/T17626.11
谐波电流(Harmonic): IEC61000-3-2、EN61000-3-2

电压闪烁(Flicker): IEC61000-3-3、EN61000-3-3

辐射干扰(Radiated Interference)是通过空间并以电磁波的特性和规律传播的。但不是任何装置都能辐射电磁波的。传导干扰(Conducted Interference)是沿着导体传播的干扰。所以传导干扰的传播要求在干扰源和接收器之间有一完整的电路连接。

产品认证专线:15017922522 Q:2355957599杨工