输入为交流200V/50HZ,
输出直流高压模式(HV):
电压:10V—3000V(峰值)
脉冲时间:1~99微妙
精度要求:+-5 V
接上模拟负载电阻后,电压不低于2850V
直流低压模式(LV):
电压:10V—500V(峰值)
脉冲时间:1~99毫妙
脉冲时间:10~990微妙
精度要求:+-1 V
以上高压两种模式输出脉冲个数:1~99可设置
请问有什么方案
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入为交流200V/50HZ,
输出直流高压模式(HV):
电压:10V—3000V(峰值)
脉冲时间:1~99微妙
精度要求:+-5 V
接上模拟负载电阻后,电压不低于2850V
直流低压模式(LV):
电压:10V—500V(峰值)
脉冲时间:1~99毫妙
脉冲时间:10~990微妙
精度要求:+-1 V
以上高压两种模式输出脉冲个数:1~99可设置
请问有什么方案