This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019 求助

Other Parts Discussed in Thread: UCC28019

UCC28019 ,设计boost PFC 电路,输出385vdc,250W;参数按照ti的计算表格计算,电路图如下,见附件。PCB和计算见附件。

在轻载时候,输出VICOMP=0.3V,VINS=2.9v,Vsense=4.3v, Vcomp=7.6v,请问该如何调整参数呢?

pfcch.zip
  • 电感用的是铁氧体 PQ40/40  感量1.7mH,有时候启动的时候能短暂的工作下输出电压升到400v,然后很快(大概十多秒到几十秒吧)的就又不工作了,输出降回320v。在400v的时候,电压不稳定。

  • 您好,确认下您所遇到的问题是不是:轻载时芯片工作不正常,不能正常升压到400V?

    1. 重载时芯片工作正常吗?
    2. 您原理图中的驱动电路有两种接法,测试中采用的是哪一种?
    3. 从轻载引脚电压上来看,芯片好像进入保护状态,请测量驱动波形,看看是否有驱动?
    4. 供电电压是12V?Pin7电容多大?从封装看,容值不大,建议增加到100uF.
    5. 如果电路不稳定,建议降低输入电压(用工频变压器把输入电压降到50VAC),输出也降到100VDC或150VDC,相应的分压电阻也需要修改,在此低压调试通过之后再逐步增大电压调试。
    6. 您的需求和EVM板功能等级类似,可参考:http://www.ti.com/lit/ug/sluu272/sluu272.pdf

    谢谢!