Other Parts Discussed in Thread: BQ40Z60EVM-578, BQ40Z60
-------
问题1:我的4个18650电芯(每个是4400mAh)接在BQ40Z60EVM-578开发板上,并且连接着EV2300,Studio软件上的FullChargeCapacity总是显示只有2600mAh左右,应该是4400 x 4 = 17600mAh左右才对吧?充放电很多次了,还是无法修正过来?这个应该怎么让他正确识别到呢?
问题2:技术手册上讲了Qmax的更新条件,是在relax态下读到OCV才更新一次QMax,Qmax是不是等同于软件界面上的FullChargeCapacity呢?另外“Ra”的全称是什么,手册里找不到?
问题3:论坛里其他网友常问到的“自动学习循环”怎么才能进入?具体方法是设置什么寄存器呢?
问题4:是不是对于每一个新电池组,化学ID都要重新计算,计算方法是把什么log文件上传到TI网站,让网站给我们计算好,是这样吗?自己用Studio软件无法更新吗?能否大致讲一下?
问题5:Studio软件中T1到T4四个温感都开启了,模式也是一致的,但是其中两个温感温度显示-273℃,怎么回事呢?它们四个应该都是差不多的问你读才对啊。
(麻烦解答,辛苦了!)