This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24045充电截止提示

Other Parts Discussed in Thread: BQ24045

在使用BQ24045给锂电池充电,有时会出现充不满的问题,表现为充满指示信号一直不给出,设置的充电电流为150ma,截止电流为5%也就是7.5ma,重新插拔充电线后充满电信号就会给出,这个是怎么回事?

另外还有个现象,充满电后拔掉充电线后再插上,会有一段时间显示未充满电(设备处于关机状态,功耗只有几十UA),这个又是怎么回事?

谢谢!

  • 这个问题有人可以解决吗?帮帮忙,谢谢!

  • 7.5mA的截止电流非常小,充满截止一定要检测到电流低于这个值才会真正截止。充电是在关机情况下,还是在设备工作的时候?如果是关机状态,有可能是有外部因素干扰了7.5mA的电流阈值判断,如果是开机,有可能是系统负载导致电流降不下来。

    可以把截止电流调高到10%试试,7.5mA时电流精度也不一定好,也会影响判断。

    至于充不满,拔电再插上就显示满了;还有充满后拔电显示不满,这个都跟这个充满阈值有关系,芯片是判断这个电流截止点的。这个点越低,判断难度就越大。