This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FCC值 BQ27541G1



各位同仁,是否有遇到BQ27541G1出现如下现象:

RM 正常

FAC值正常

FCC值在放电的时候不变,在电池静止状态也不变化(例如都为8800mAH ),但是在充电时FCC就逐渐减小,(大概减小比例在10——30%),然后随着RM值的增加,FCC减小到与RM相等(例如6000mAh),然后FCC与RM值就一同增加,直到检测到满充状态(例如就增加到8700mAh)。

这样就造成SOC显示的百分比会提前达到100%(例如RM为6000mAh就为100%),实际上电池是没有充满的。

麻烦TI的专家和各位同仁帮忙分析下是什么地方出了问题

谢谢!