Other Parts Discussed in Thread: UCC3803, LM5001, LM5000, TPS40210, TPS55340
输入:9-32Vdc,
输出:5Vdc,
频率:100k左右
要求隔离式,可长期空载、长期短路。
是否有相关控制IC?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以采用电流模式控制芯片UCC3803: www.ti.com.cn/.../ucc3803
如果功率不大,或者你可以采用LM5001这样的芯片,见datasheet: www.ti.com.cn/.../lm5001.pdf FIGURE 7. Isolated Flyback 可以参考,不同的只是输入电压的差异,可以修改一下变压器。
UCC3803没有这样的设计案例,选用这个芯片是因为它的低启动电压,以及可以设计为flyback架构。
TPS40210这款芯片可以做成反激,见文档: www.ti.com.cn/.../slyt302.pdf 第二页。
这个方案是可以实现5V, 1.5A输出的
或许你可以参考TI的PMP5063方案: www.ti.com.cn/.../slur389.pdf
和你的应用条件很相似,只需要将输出电流设计大一点就可以了。
LM5001的开关电流只有1A,勉强可以做到输出5V/1.5A。
LM5001的开关电流只有1A,设计时按照下限0.8A设计,确实不足以做到输出5V/1.5A。
TPS55340, TI有提供8~24V转5V/2.5A的方案,您可以参考: www.ti.com.cn/.../getliterature.tsp
(TPS40210的方案挺好的)
LM2578-ADJ也是可以的,见10~30转5V/2A的方案: www.ti.com.cn/.../getliterature.tsp
LM2578是5A的开关电流,可以选择LM2585-ADJ ,是3A开关电流。