现在焊接了一块TPS65217C的板子,上电测试发现1.8V输出端为1.9V,3.3V输出4.4V ,1.5V和1.1V均输出正常,没有出现短路的情况
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在焊接了一块TPS65217C的板子,上电测试发现1.8V输出端为1.9V,3.3V输出4.4V ,1.5V和1.1V均输出正常,没有出现短路的情况
你好,
因为LDO 结果不准所以怀疑是LDO部分有问题,重新焊接一块是不是也是同样的现象。
现在将LDO1的3.3V与LDO2的1.8V调好没问题了,所有的DCTODC也没问题,就是LDO3输出3.8V、LDO4输出4.4V输出异常的问题没找到?原本LDO3与4正常输出的电压范围是1.8-3.3V 啊,现在超出范围了,是否有可能电源芯片LDO3、4那部分坏了?
LDO1带上负载VRTC后就正常了,输出1.8V,之前没接负载输出1.9-2.0V左右,但是LDO3、4一直不正常