目前正在应用INA226来测试电流,发现连个问题。
1. 如何确定INA226的电流精度?在Datasheet里面如何得到理论测试精度是多少?
2.在测试电流时,在连续的读取中电流读取值会慢慢变大,实际的被测电流是一个恒定电流源。增大幅度为3mA每秒。
请帮忙解疑答惑谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
很大的电流有可能是采样电阻发热引起的,所以如果稳定一段时间后不再增加,并且散热可以降低,那么提高精度的方法是使用低温漂的电阻,像专用于电流测量的shunt电阻。