现在我需要设计一个给ADS1243供电的隔离电源,电源输入12V,输出要求5V,200mA,由于是使用高精度的AD所以对电源要求比较高,购买的现成的DCDC发现噪声和纹波较大,在80~100mV左右,频率在1M~1.5M,请问这个噪声+纹波对我的AD影响多少?
另外请问,如果我重新设计一款隔离电源,有什么好的应用方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC的电源可以不用到隔离电源(隔离一样存在噪声),见附件文档,有关于ADC电源设计,关于噪声影响的方案比较,你可以参考。
之所以使用隔离电源是因为之前的一款设计中没有采用隔离,因为板子上又继电器,继电器吸合时会造成AD的死掉,所以之后的设计都采用隔离电源,隔离芯片,但之前是采用的变压器输出两路隔离电压,但这次是使用1路电源,所以需要采用隔离电源,隔离芯片使用ISO7242
如果采用隔离电源,可以选择LM5001: www.ti.com.cn/.../getliterature.tsp 见datasheet第十六页参考方案,因为你的输入电压时12V,所以需要修改一下变压器规格。(5V输出后仍可参考上述文档的设计)
如果没有价格上的忧虑,可以使用DCR011205: www.ti.com.cn/.../getliterature.tsp
7805也是LDO, 或者你可以选择低noise, 高PSRR的LDO, 如200mA的TPS79901 ,TPS73401;500mA的,TPS79501,TPS73501. (可以在TI官网上申请样片: www.ti.com.cn/.../homepage.tsp)
7805针对noise 的特性上没有上述推荐的好,同时还可以增加一些RC/LC来进一步改善噪声效果。
经测试发现这个噪声是由我使用的IB1212ls产生的,噪声+纹波 峰峰值在100mV,频率在1M~1.5Mhz,采用一个无源的滤波器能否滤除这个频率?采用哪种滤波?参数怎么计算?