BQ25895的内置算法可以与QC3.0的充电头实现握手并快充锂电池吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ25895的D+D-内置的只支持9V/12V这种档数比较少的高压握手协议,如果需要灵活的可以看一下BQ25890H,D+D-的电压都是灵活可调的
请问BQ25895 的DSEL引脚是怎么使用的,要外界单片机识别D+D-吗?
Hi Zeyuan
BQ25895 与 BQ25890H都是可以支持QC3.0充电的,
BQ25895支持9V/12V 的默认电压配置,BQ25890H可以支持QC3.0的多级调压。
谢谢!
请问是需要外接单片机才能实现QC3.0握手,还是直接利用芯片上D+D-就可实现。