This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2909ep中温度补偿的问题

Other Parts Discussed in Thread: UC2909-EP

您好,咨询两个关于UC2909-EP温度补偿问题:

1)请问UC2909中的内部参考电压2.3V@-0.39mv/℃,这个是与输出电压反馈调整后的电压进行比较,是如何能实现对输出电压能达到-3.9mv/℃的调节的?

2)如果需要调节输出电压随温度变化率为-4mV/℃,该如何实现。

期盼您的技术支持,非常感谢!

  • PDF中介绍的很明确,通过一个10K的热敏电阻接地,可以实现-3.9mV/°C的调整啊。

  • 谢谢您的回复,PDF中确实是例图中这样给出的,我的问题是我不理解是怎么做到这种补偿的,因为热敏电阻改变的的参考电压2.3V,而参考电压是与输出成比例的反馈电压进行比较,不是与输出电压直接比较,最终是如何保证输出电压按-3.9mv/℃调整的呢