This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1不能自动停止充电



原理图如下,

1、我插充电器给电池充电的时候,通过BQ studio软件配置充电MOS管打开,放电MOS管是关闭的,就是原理图里面左边的MOS管,右边的MOS管关闭可以开吃充电,我配置的Charge Term Taper Current是600mA;实际充电到电流200mA的时候还是没有停止充电,并且我是满足Valid Charge Termination条件的,但是却没有停止充电。

2、我实际板子上测量CHG,和DSG这两个管脚,充电时我只打开了充电MOS的管,但是放电MOS管也被打开了。

3、是否我软件参数配置不正确,导致不能按照设置条件停止充电了。

thankyou