Other Parts Discussed in Thread: LM5060
在使用LM5060的时候,过压(36V)和欠压(19V)都调试OK,RS=1K,RO=0R,MOSFET Rds=3.0mΩ 电流设定为大约5A, 这部分也OK。
但输出短路时,示波器测量TIMER脚(0.1uF)峰值为1.5V,达不到2V,LM5060不会关闭MOSFET,MOSFET反复开关导致发热烫手。
求此问题的原因和解决方法。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请问此时EN, VIN, UVLO这三个pin脚波形是如何的呢?
Regards,
Patrick