This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92690做摄影灯方案输入DC9-28V 输出DC45V恒流1A



各位大师、专家们好,小弟手上有一个LED照明摄影灯的案子功率是50W,客户要求实现两路LED色温分别调光混色额外再增加一路外置PWM(频
率67KHz) 调光,芯片Datasheet介绍PWM调光可以支持2M的调光频率,请问这颗芯片用67KHz的PWM调光信号控制输出LED灯的电流是线性均匀变化吗?

  • 您好,

      PWM调光的原理就是通过一定频率的开关,通过改变占空比大小来获得等效的输出电流(LED驱动电流),因此LED灯的电流是可以实现线性均匀变化的。谢谢

    Regards,

    Patrick

  • 好的,非常感谢你的回复,另外这个PWM调光频率是67KHz应该没有问题吧!

    另外还请帮忙推荐一个DC/DC的快充方案给我,输入是Micro USB 支持QC 2.0、3.0 电压 5V、9V、12V和20V四档充电电压  ,输出4.2V/2A、3A ,谢谢!