各位工程师,大家好,小弟最近要做一款TL3843的反激电源。在看官方datasheet的时候有以下两个疑问:
1,It is good practice to use one standard via per 200 mA of current if the trace will need to conduct a significant amount of current from one plane to the other。这句话出现在手册的13页,10节layout。请问下这个标准过孔是多大的内径,外径又是多大呢?
2,如下图中红色画圈处,这里的圆圈是数字电路中的非功能吗?如果是要怎样理解,1V经过非后是多少?然后在低于1V后非又是多少?还有这个比较器没有标注正负输入。为啥还要加一个非门在这里,如果去掉非门,在设计的时候直接把比较器的正负输入交换不也一样吗?还有TL3843内部数字逻辑门是TTL电平还是CMOS电平。很多疑惑啊。还请TI工程师们帮一下忙。在下感激不尽。