This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24193 充电电流一直为0,不能充电

Other Parts Discussed in Thread: BQ24193

我现在使用贵公司BQ24193 快充芯片,遇到以下问题:
问题1:快充无法对电池充电
充电时,电池电压有4.2v的充电电压,读取芯片reg08查询充电状态一直是“10 – Fast Charging” 和 “11 – Charge Termination Done” 不断切换,但就是电池充不进电;
问题2:充电时BQ24193的INT关键不断的触发一个低电平信号。
锂电池特征为:标称电压:3.8V;  功率:L7000mAh/26.6Wh;  充电限制电压4.35V
运行平台是hi3519,并且我能够读取到芯片的寄存器状态为:
REG00: 0x37 00110111
REG01: 0x1b 00011011
REG02: 0x60 01100000
REG03: 0x11 00010001
REG04: 0xb2 10110010
REG05: 0x8a 10001010
REG06: 0x03 00000011
REG07: 0x4b 01001011
REG08: 0xb4 10110100
REG09: 0x00 00000000
REG10: 0x2f 00101111