This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

稳压芯片与仪表放大器配合使用出现错误!请求帮助!!!



使用TPS78915和TPS78930两款芯片与仪表放大器配合使用。

仪表放大器采用单电源供电,TPS78930的输出端接仪表放大器的正电源端,TPS78915的输出端接仪表放大器的REF端。TPS78915和TPS78930的输入端同时接入外部供电端约为3.5V。TPS78915和TPS78930的外部电容就按照芯片手册上的推荐接法连接。

连接好电路后发现仪表放大器不能正常工作。使用万用表测量电压,TPS78930可以正常使用,输出电压约为2.9V。TPS78915输出电压不正常,约为2.6V。

为了解决此问题进行了以下三次试验:

1.按照芯片手册上的推荐接法单独连接TPS78915,输入约为3.5V,输出约为1.5V,可以正常工作。

2.连接仪表放大器,去除TPS78915,保留TPS78930。使用万用表测量电压,测得REF端电压约为2.9V,与TPS78930的输出电压相当。

3.连接仪表放大器,去除TPS78915,保留TPS78930,使用台式电源为仪表放大器的REF端供电1.5V,此时仪表放大器可以正常工作。


由以上试验可以得出哪些结论呢?

TPS78915不能为仪表放大器提供REF电压吗?

哪款芯片可以为仪表放大器提供REF电压呢?

选择线性稳压芯片时应该考虑哪些方面呢?

恳请各位专家、大神抽空能给解答一下!

O(∩_∩)O谢谢~