This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题
Full Charge Capacity (FCC) and Remaining Capacity (RM) are both compensated values which depend on the rate, temperature, and impedance of the battery. This is different from Full Available Capacity (FAC) and NomAvailCap (NAC) which assume nominal temperature and a very light load. If at rest, FCC and RM will usually be calculated by the gauge by running a simulation at the current temperature assuming a load equivalent to Avg I/P Last Run (in dataflash).
实际电量参考FCC
你好
1、上面这段英文是自己写的还是摘自哪篇文档?如果是文档,帮忙把这篇文档分享下谢谢!
2、FCC 与FCC True ,RM 与RM True啥关系?
3、我给G27510施加800mA的电流负载,流量计显示的是890mA,是不是校准出现了问题?
2. FCC true和RM true可根据真实的电流充放电积分进行计算,计算方法在如下链接中:https://e2e.ti.com/blogs_/b/fullycharged/archive/2016/11/04/how-accurate-is-your-battery-fuel-gauge-part-2-2。
3. 是校准出现了问题,需要校准成功之后才可进行其他操作。
27510G3充电显示100%跟亮绿灯间隔时间很长,最短的也有半个多小时,长的能达一个多小时,这个跟什么因素有关?如何缩短?充电芯片的截止电流为78mA,目前设置Taper Current 为100mA