This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25121疑问



Hi
1:实测,precharge到fast charge的阈值电压是3.15V,不是手册里说的3.0V,我在precharge=4mA和2.4mA下都测试了,怎么回事?
 2:当MCU的I2C失效后,由于无法喂狗,芯片会复位,但是实测LDO不会掉电,而是直接从3V掉到默认的2.5V,导致MCU也无法复位I2C,且这时使用MR复位无效。现在想到的办法是,能否让RESET引脚直接连到MCU,然后让MCU复位,就可以重置I2C了。所以想确定下,I2C失效后,RESET引脚已经会不会输出低?
3、不用TS功能的话,能否将TS下拉电阻去掉,直接上拉10K到VIN?
谢谢!
  • 你好,

    1. BUVLO的值可以在bq studio中配置,从2.2V到3.0V,可以直接测BAT端电压。同时方便的话可以上传相应的波形图,以便分析。

    2. 看门狗超时的话,LDO是处于disable状态的,所以可以直接复位MCU。你是用外部电阻设置IPRETERM/ISET/ILIM三者的值吗?还是用I2C直接写寄存器设置?如果同时使用外部电阻及I2C设置的话,两者的值会干扰IC的复位状态。

    3. 如果TS 端不用的话,需要通过电阻分压网络,将TS端的电压值设置在55%--60%Vin,详见数据手册P11.

    谢谢。