This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24195的使用问题

Other Parts Discussed in Thread: BQ24195

我想用BQ24195来对锂电池进行充放电管理,请问:我是否可以通过I2C接口来读取电池组的实时电压值,这样我可以通过电池组的电压值大概了解电池组的电量状况,对电池电量状况实现粗略监控。

    • 可以看一下24195的手册中,有没有读取电池电压的寄存器,如果有对应的寄存器就可以读取
    • 使用电压估算电量精度很低,建议还是使用专门的gauge芯片检测电量

  • 您好。我看到手册中的REG04 (Chanrge Voltage Control Register),读取这个值,是否就是当时电池电压的值呢?

    当然,在我的应用中,不需要精确估计电池电量,只需要大概示意一下就可以了。

    谢谢。

  • 另外,从其他学友那里听说,如果需要测量电池电压,需要先关闭Q4,这是为什么?

    我的应用需求是:准备采用USB接口进行电池充电,不需要OTG功能,负载是一个宽电压设备(3~10V都可以工作,电流小于1A),也就是说可以不需要任何升降压功能,请问我的负载接到那个端口比较合适?怎么简化手册中的参考电路?