我使用LM5002把12V升压为48V,单路如下图。
负载是MIC(麦克风),电流最大十几mA,现在的问题是纹波比较大,接近10V(波形如下),请帮忙分析一下原因。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用LM5002把12V升压为48V,单路如下图。
负载是MIC(麦克风),电流最大十几mA,现在的问题是纹波比较大,接近10V(波形如下),请帮忙分析一下原因。谢谢!
首先你测量纹波的方法不对, 示波器探测笔形成的环路尽可能小,避免引入噪声,同时带宽选为20MHz。
其次请同时测量SW波形和输出纹波,共同显示
建议换一个反向恢复电荷Qrr较小的肖特基二极管
你好,
1.建议使用四层板,用第一第三层来走线以达到较好的shielding效果
2. SW点包含高频噪声,相当于一个噪声源,因此布线时SW node area应该尽量小
3.对boost电路来说,由D1和输出电容C7、C8和SW node组成的loop由于存在很高的di/dt,因此这个loop在布线时越小越好,从而降低寄生电感,减小高频噪声
4. FB对噪声敏感, 布线时此线路应该远离噪声源