This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO的高温老化实验问题请教(TPS736xx)



打算利用TPS736xx做一个电路,这块板需要做125度高温老化实验,输入3V,输出1.5V,正常工作功耗30mA,启动电流达到300mA,采用DCQ封装,计算温升有6度。

问题来了,芯片最大绝对温度是150度,推荐工作温度是-40到125度,在做高温老化实验时芯片结温会达到131度,要做1000个小时的实验,请问这个芯片还能不能用?

不想使用汽车级的芯片和航天级的芯片,因为太贵了。