看中了TI的BQ76930可以管10片,想用2片级联,但是这个片子不能级联。
如果想2片级联,I2C要怎么级联? 另外还想电量统计,2个BQ76930要怎么接,芯片BQ78350 BQ34Z100 这些。电阻均衡。
有参考设计吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看中了TI的BQ76930可以管10片,想用2片级联,但是这个片子不能级联。
如果想2片级联,I2C要怎么级联? 另外还想电量统计,2个BQ76930要怎么接,芯片BQ78350 BQ34Z100 这些。电阻均衡。
有参考设计吗?
感谢TI的工程师。
有两种方案要做,一种是20串的锂电80V应用,原先用TI 100V的TPS7A4001做的耐压100V的。如果2片76930带上各类芯片,通信,以及其他,可能不够了,要换BUCK芯片耐压100V的。这个电量统计的芯片
还一种就是13串15串锂电应用,对应48/60V ,这个用76940应该也可以了。
这个电量统计的芯片,耐压到65,15*4.2V=63V 耐压到顶了。 如果是20串应用是要配置2片电量计了吧,总的是2片电量的累加吧?
看了下市面上现在电动工具的20串80V应用的芯片比较少,可能应用比较少,厂家方案也没有多少吧。
请参考下面的TI Design
http://www.ti.com/tool/TIDA-01093?keyMatch=bq76930&tisearch=tidesigns
High serial cell count battery (>15s) systems are becoming more and more common for industrial applications. These applications are cost sensitive and require a simple solution that includes monitoring, protection, and control or even SOC (State of Charge) information rather than only basic independent hardware protection. This design offers a platform for the complete pack side solution. All independent hardware protection features are incorporated from the bq76930 and a robust communication interface is implemented for host device to read the battery information.
您好,链接中的MSP430G2955处理器,换用成BQ78350-R1,能行的通吗?还有BQ76940能否用使用这样的级联模式。谢谢!
BQ78350-R1不能支持两个BQ76930或BQ76940啊
78350+76930保护板在先接入充电器,再对充电器接入市电时,保护板瞬间进入短路保护状态,并持续。如果先将充电器接入市电在将充电器接到保护板时可以正常充电;
78350+76930保护板接纯电阻负载不会出现短路现象,但是接入其他类型的负载时会出现持续短路状态。
我的保护板是按照参考电路设计的,在充放电回路有些电容是没有按照参考来设计
78350+76930保护板在先接入充电器,再对充电器接入市电时,保护板瞬间进入短路保护状态,并持续。如果先将充电器接入市电在将充电器接到保护板时可以正常充电;
78350+76930保护板接纯电阻负载不会出现短路现象,但是接入其他类型的负载时会出现持续短路状态。
我的保护板是按照参考电路设计的,在充放电回路有些电容是没有按照参考来设计