This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51216输出问题

Other Parts Discussed in Thread: TPS51216, CSD87331Q3D

设计目标:

        输入电压:5V

        输出电压:1.8V

       输出电流:4A 最大

电路图如下:

问题现象:

首先将S3和S5置高,

测得电感后级输出稳定在0.736V,没有达到1.8V。使用万用表测量时,显示先到过1.8V后马上下降为0.736V

由于VLDOIN是接在1.8V上的,导致VTT和VTTREF都没有输出0.9V。

VREF输出电压为1.823V,VREFIN的电压也为1.823V。后将VREFIN的电压分压到1.5V,后级输出还是0.736V。

1.请问反馈电阻R477设置为10K,R478不焊接是否正确?

2.MOS管Vin接5V是否会影响输出?

3.电感取值是否合理?

对比了参考电路slur270.pdf中page7没有发现很大的区别,请指出设计中可能存在的问题,谢谢