This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60芯片,自己做的板子,充电故障,麻烦分析一下!

Other Parts Discussed in Thread: BQ40Z60

---

----

----

-------------

自己做的板子,用的BQ40Z60芯片,目前存在“充电过慢”问题,具体现象如下:

在PreCharge阶段,电流大小很好,和设置的电流值一致(默认的),到了LV充电阶段,刚开始电流大小也很好,1900mA左右,不过只能维持1分钟不到,然后开始锐减,3、5分钟内电流就会逐步减小到40mA,然后就一直这样了,充电非常慢。而且基本上是左边仪表盘电压升到13200mv左右就开始下降了,正常这个电池组充满能到16000mv以上。放电没问题。

仔细看了一下,在设置里,并没有限制充电电流啊,而且各种温度都很好,也没有什么安全告警,试了很多回都是这个规律。同一个电池组,用TI的官方评估板就不存在此问题(都是BQ40Z60),各种设置都和评估板上的芯片配的一致啊。上传了几个图,麻烦TI工程师分析一下。

另外我再问一下关于LearningCycle的几个问题:

1、LearningCycle的流程顺序到底是什么呢?之前有TI工程师回复说“先IT ENABLE , 先充满, FC置位, 静置2小时, 再恒流负载C/5对电芯放电到空, 静置5小时 ,Update Status由04 变为06或者0E”,那我开启LearningCycle的时机是位于哪里?

2、想我这个帖子的症状,充电很慢,要好几天才能充满,那我怎么才能进行LearningCycle啊?

3、“放电到空,静置5小时”,放到空是指FD刚一置位就立刻要停止放电吗?不能使劲放直到软件都连不上芯片是吧?

4、LearningCycle一开启,此页面的左下角就有无响应的提示,这说明了什么?转换到其它页面无此提示。

 

感谢TI工程师们。